ADC conversion clock cycles

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC conversion clock cycles

2,507 Views
TEMCEFF
Contributor IV

Hi, 

I got a small doubt. In LPC1768/69 ADC is SAR type. for a 12 bit resolution, it should take 12 cycles for complete conversion. But in user manual mentioned that,

A non-burst mode conversion requires
65 clocks and a burst mode conversion requires 64 clocks. 

Can you explain this?

Regards,

Muralidhar.

Labels (4)
0 Kudos
Reply
2 Replies

2,390 Views
TEMCEFF
Contributor IV

Anyone can help me on this.

0 Kudos
Reply

2,390 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Avinash,

Regarding your question that the ADC conversion time of LPC17xx requires 64 clock cycles based on SAR mechanism, it is said that the ADC converter of LPC17xx is initial version, for the later ADC converter for example the ADC of LPC54xxx, the ADC is optimized, the ADC clock frequency becomes higher, the conversion time becomes shorter.

BR

Xiangjun Rong

0 Kudos
Reply