ADC LOWPRIO bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC LOWPRIO bit

1,986 Views
ianbenton
Senior Contributor I

Could you please clarify the action of the LOWPRIO bit in the SEQA_CTRL register.

The manual says that it sets the priority for sequence A.

In low priority mode, any SEQB trigger is ignored  - thus SEQA has higher priority.

In high priority mode, the SEQB trigger interrupts the SEQA sequence, and the SEQA sequence has to wait until the SEQB sequence is completed before it can resume - thus SEQA has lower priority.

This seems completely contradictory to the description.

Please advise.

Labels (2)
0 Kudos
Reply
3 Replies

1,897 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Ian Benton ,

I also think the name "Low priority" "High priority" may be misunderstood.

While the real function of this bit please refer to the clarify:

pastedImage_1.png

Hope it helps,


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,897 Views
ianbenton
Senior Contributor I

Are you going to correct the manual?

0 Kudos
Reply

1,897 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Lan,

I will report it document team, while I'm not sure whether it will be changed .

BR

Alice

0 Kudos
Reply