• ACSafe10.axf: Error: L6220E: Load region LR_IROM1 size (57352 bytes) exceeds limit (57344 bytes). Region contains 34 bytes of padding and 248 bytes of veneers (total 282 bytes of linker generated content).

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

• ACSafe10.axf: Error: L6220E: Load region LR_IROM1 size (57352 bytes) exceeds limit (57344 bytes). Region contains 34 bytes of padding and 248 bytes of veneers (total 282 bytes of linker generated content).

5,171 次查看
steve_young1
Contributor I

All,

I just starting getting this linker error when adding new code to an existing LPC2132FBD64/01 project.  I believe it means there is no more code space available, is this correct?

I am using Keil ARM Basic 4.1 and the target options are set as RO Memory area IROM1: 0x2000 len 0xE000.  Are these values correct for allotting all available code space?

Any suggestions for squeezing a bit more into this processor?

Thanks in advance.

0 项奖励
回复
0 回复数