A problem about program the SDK example of Keil to externall flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A problem about program the SDK example of Keil to externall flash

3,466件の閲覧回数
827529957
Contributor III

I have read the "Getting Started with MCUXpresso SDK for LPC540xx.pdf " in the SDK package directory "SDK_2.6.0_LPC54S018_MDK\docs", which has a section on how to program the non-XIP (plain load) example application to external flash using J-Link.

There is a step that makes me confused.as shown below,The Start address in the red box in the figure is 0x00000000. Does this mean that the address to be programmed is SRAM, not external flash?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,363件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  Kunsen Chen,

"Does this mean that the address to be programmed is SRAM, not external flash?"

-> No, this is programmed to external flash.

Could you please refer to this DOC to have a test, program it, re-power your chip, check whether it download

into external flash. Waiting your result. 

3,363件の閲覧回数
827529957
Contributor III

Thank you for your reply. I did test it as you said and found that the program can still run after re-powering. I tried to use JFlash to read the binary data of the external flash and can actually read the code data.

0 件の賞賛
返信

3,363件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

OK, thanks for your sharing.

0 件の賞賛
返信