A problem about program the SDK example of Keil to externall flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A problem about program the SDK example of Keil to externall flash

3,525 Views
827529957
Contributor III

I have read the "Getting Started with MCUXpresso SDK for LPC540xx.pdf " in the SDK package directory "SDK_2.6.0_LPC54S018_MDK\docs", which has a section on how to program the non-XIP (plain load) example application to external flash using J-Link.

There is a step that makes me confused.as shown below,The Start address in the red box in the figure is 0x00000000. Does this mean that the address to be programmed is SRAM, not external flash?

Labels (1)
0 Kudos
Reply
3 Replies

3,422 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  Kunsen Chen,

"Does this mean that the address to be programmed is SRAM, not external flash?"

-> No, this is programmed to external flash.

Could you please refer to this DOC to have a test, program it, re-power your chip, check whether it download

into external flash. Waiting your result. 

3,422 Views
827529957
Contributor III

Thank you for your reply. I did test it as you said and found that the program can still run after re-powering. I tried to use JFlash to read the binary data of the external flash and can actually read the code data.

0 Kudos
Reply

3,422 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

OK, thanks for your sharing.

0 Kudos
Reply