4370 ISP "boot"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

4370 ISP "boot"

938 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Thu Sep 18 15:43:19 MST 2014
I am interrested in the LPC-Link2 board (4370)

If I enter ISP mode (with a low on the appropriate pin at reset) and write a program image
to sram at 10000000, and then 'Go'

What is to state of (a) the M4MEMMAP register and
(b) clock speed, clock source, PLL1 settings etc.

Do I have to transfer to an actual code address and setup my own SP,
or would a transfer to 1000000 take this as the vector table and set the
stack and initial PC from the first two entries?

Regards, MIke
Labels (1)
0 Kudos
Reply
0 Replies