whether KSDK support K60DN512Z ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

whether KSDK support K60DN512Z ?

1,444件の閲覧回数
zzyy
Contributor I

hi, everyone. I want to know whether KSDK support K60DN512Z ? I only found K60D512xxx10. What should I do ? thank you.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,337件の閲覧回数
santiago_gonzal
NXP Employee
NXP Employee

Hello,

If you are going to begin a new SW development, K60DN512 is supported in the KSDK and is pin to pin compatible with K60DN512Z, so it's highly recommended that you use the new device, which improves some peripherals and fixes silicon issues.

You have all the changes between both devices here:

http://cache.freescale.com/files/32bit/doc/app_note/AN4445.pdf

Regards,

Santiago

0 件の賞賛
返信