is there some example using frdm-k64f + kds3.0+ PE+ sdk 1.2 + lwip?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

is there some example using frdm-k64f + kds3.0+ PE+ sdk 1.2 + lwip?

1,412件の閲覧回数
matherinewang
Contributor III

there is a offical demo for lwip, but the demo project without PE components, i need new a project using PEx and SDK, does anybody have a example for that? thanks in advacne!

ラベル(1)
1 返信

1,104件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello matherinewang,

Yes, you can inspire by this project Re: Re: Assistance needed with lwIP + PEx + KSDK

It is created in KSDK 1.1 and KDS 2.0. + PEx (for frdm-k64f)

Other PEx examples with KSDK 1.2 for ADC, GPIO, PIT, RTC and UART you can find at installation folder for KDS,

C:\Freescale\KDS_3.0.0\eclipse\ProcessorExpert\Repositories\KSDK120_Repository\Projects\Kinetis\Processor_Expert_SDK\FRDM-K64F120M\GCC

I hope it helps you,

Have a nice day!

Iva