Could someone working on the next version of the Kinetis Connectivity Software SDK make sure that all of the headers are conditionally-wrapped for C linkage?
#ifdef __cplusplus extern "C" { #endif ... #ifdef __cplusplus } #endif
This isn't currently the case with most of the headers from the v1.0.2 Connectivity Software SDK.
Not exposing using C linkage leads to the usual errors when called from C++ files:
./source/Coordinator.o: In function `MLME_NWK_SapHandler(nwkMessage_tag*, unsigned long)': /../source/Coordinator.cpp:929: undefined reference to `ListAddTailMsg(list_tag*, void*)' ./source/Coordinator.o: In function `MCPS_NWK_SapHandler(mcpsToNwkMessage_tag*, unsigned long)': /../source/Coordinator.cpp:937: undefined reference to `ListAddTailMsg(list_tag*, void*)' ./source/Coordinator.o: In function `App_init': /../source/Coordinator.cpp:964: undefined reference to `ListInit(list_tag*, unsigned long)' /../source/Coordinator.cpp:965: undefined reference to `ListInit(list_tag*, unsigned long)' /../source/Coordinator.cpp:968: undefined reference to `Mac_SetExtendedAddress(unsigned char*, unsigned long)' ./source/Coordinator.o: In function `AppThread(void*)': /../source/Coordinator.cpp:1017: undefined reference to `ListRemoveHeadMsg(list_tag*)' /../source/Coordinator.cpp:1150: undefined reference to `ListRemoveHeadMsg(list_tag*)' ./source/Coordinator.o: In function `coordinator_main_task': /../source/Coordinator.cpp:1203: undefined reference to `TMR_Init()' /../source/Coordinator.cpp:1205: undefined reference to `SecLib_Init()' /../source/Coordinator.cpp:1208: undefined reference to `RNG_Init()'
I've added this wrapping to copies of the headers in my project (cloned with the Project Cloner), but it would be great to see this upstream.