Hi Ari,
The Freescale Kinetis SDK_1.3.0 standalone for KV4x MCUs via TWR-KV46F150M is available on www.freescale.com . The Download button lead you to the Kinetis SDK Flexnet.
o Installers are in “KSDK v1.3.0 Standalone releases” item:
Installer: Kinetis SDK1.3.0 Standalone for KV4xF via the TWR-KV46F150M – Windows
Installer: Kinetis SDK1.3.0 Standalone for KV4xF via the TWR-KV46F150M – Linux
Installer: Kinetis SDK1.3.0 Standalone for KV4xF via the TWR-KV46F150M - Mac OS
MQX™ RTOS support for the TWR-KV46F150M Freescale Tower System module.
The Kinetis SDK is intended for use with Freescale’s Kinetis MCU product family based on the ARM Cortex-M series architectures. The release consists of:
o Kinetis MCU platform support
o Demo applications/Driver examples
o The FatFs FAT File System
o RTOS support components
o Documentation (Kinetis SDK API Reference Manual and various user’s guides)
Please consult the release notes.
Hope that helps,
Have a great day,
Kan
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------