When can we expect KSDK release with lwip 2.0.0 integrated?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When can we expect KSDK release with lwip 2.0.0 integrated?

3,198件の閲覧回数
deeptimoodliar
Contributor II

This latest lwip (2.0.0) release has some good features which we would like to have.

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

3,014件の閲覧回数
Jmart
NXP Employee
NXP Employee

Deepti - You can find lwip 2.0.0 support in our platforms that were released with release 5 (this is a subset of the overall supported SoCs). If your platform was not in the release 5 release, you can expect lwip 2.0.0 for your platform in release 6, coming in March 2017.

0 件の賞賛
返信

3,014件の閲覧回数
deeptimoodliar
Contributor II

Hello Jason,

I am working with FRDMK64F board and have been using SDK_2.0_FRDM-K64F past few months. From nxp website, today I downloaded the latest SDK for my board: SDK_2.1_FRDM-K64F. But I am not clear what you mean by release  5. I could not find it.

Also, in the SDK2.1, I did find that lwip 2.0.0 was supported but its not the lwip 2.0.0-final release(released on 10 nov-2016). It is lwip 2.0.0 RC0. When you say lwip 2.0.0 is supported in release 5 and the release 6 coming in March 2017, do you mean lwip 2.0.0-RC0 or  lwip 2.0.0-final release?

0 件の賞賛
返信

3,014件の閲覧回数
butok
NXP Employee
NXP Employee

100%, the lwIP 2.0 final release will be available in the next public KSDK rel. 6 (2017).

Best regards,

Andrey Butok

0 件の賞賛
返信