When can we expect KSDK release with lwip 2.0.0 integrated?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When can we expect KSDK release with lwip 2.0.0 integrated?

3,130 Views
deeptimoodliar
Contributor II

This latest lwip (2.0.0) release has some good features which we would like to have.

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,946 Views
Jmart
NXP Employee
NXP Employee

Deepti - You can find lwip 2.0.0 support in our platforms that were released with release 5 (this is a subset of the overall supported SoCs). If your platform was not in the release 5 release, you can expect lwip 2.0.0 for your platform in release 6, coming in March 2017.

0 Kudos
Reply

2,946 Views
deeptimoodliar
Contributor II

Hello Jason,

I am working with FRDMK64F board and have been using SDK_2.0_FRDM-K64F past few months. From nxp website, today I downloaded the latest SDK for my board: SDK_2.1_FRDM-K64F. But I am not clear what you mean by release  5. I could not find it.

Also, in the SDK2.1, I did find that lwip 2.0.0 was supported but its not the lwip 2.0.0-final release(released on 10 nov-2016). It is lwip 2.0.0 RC0. When you say lwip 2.0.0 is supported in release 5 and the release 6 coming in March 2017, do you mean lwip 2.0.0-RC0 or  lwip 2.0.0-final release?

0 Kudos
Reply

2,946 Views
butok
NXP Employee
NXP Employee

100%, the lwIP 2.0 final release will be available in the next public KSDK rel. 6 (2017).

Best regards,

Andrey Butok

0 Kudos
Reply