Valt on fsl_adc KSDK (Voltage reference module for KSDK?)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Valt on fsl_adc KSDK (Voltage reference module for KSDK?)

1,699件の閲覧回数
holyhope
Contributor III

Hi to all,

I'm developing with KSDK 1.1.0, KDS 2.0.0 on K20 up with KSDK (using K60 uP inside KSDK)

Developing and debugging some problem on adc I want try to use the internal Vref for ADC instead my external reference.

I set to PEx "Valt" in "reference voltage" but I can't set o modify the Alternate Voltage.

I not see any KSDK Voltage Reference componente.

What I can do to modify my Valt ? So I can use that in fsl_adc component...

 

Thanks,

Massimiliano

ラベル(1)
0 件の賞賛
返信
1 返信

1,548件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Massimiliano Sturla,

      Please tell me the full name of your K20.


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信