Sense USB cable connected FRDM-K64F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sense USB cable connected FRDM-K64F

3,991 Views
giacomopetrini
Contributor IV

Using KSDK 1.1, KDS 2.0

 

I'm developing a data-logger using the FRDM-K64F

Basically I want a "double" application:

- normal behavior: data logging

- alternate behaviour, when program starts with USB cable connected (to the K64F USB connetor): MSD (so I can read the files saved on the SD card when in data-logging mode)

 

The data logging works, and I tried the MSD example (and it works).

 

Now I'm trying to merge the two.

 

What I wish to do is choose between the two mode at startup: if the USB cable is not conneted -> datalogging, if the USB cable is connected (so the board is connected to a PC) -> MSD.

 

Some ideas how to do that?

 

Thanks Regards Giacomo

 

PS: what throughput I should expect tranfering data from the SD card to a PC (using USB-MSD)?

Labels (1)
6 Replies

3,378 Views
ivadorazinova
NXP Employee
NXP Employee

Hi giacomopetrini,

you may check power on usb (if is connected to computer or if you need power supply).

Look at the schematic FRDM-K64F http://cache.freescale.com/files/microcontrollers/hardware_tools/schematics/FRDM-K64F_SCH.pdf

j3_pin10.png

Pin 10 on connector J3, page 4. Connect to any pin but through a voltage divider. And the voltage divider connect to any pin and check log 1 or log 0.

You need the voltage divider because the pins are not 5V tolerant and must be here 3.3V maximum.

And with your SD card - you can rewrite the SD - like USB Stack and with the second USB you can send the data away.

I hope it helps.

Iva

0 Kudos
Reply

3,378 Views
giacomopetrini
Contributor IV

Hello,

thanks for the tip, butI can't use it because on top of the FRDM-K64F there is a "shield" that I designed and it would be difficult to access the P5V_USB pin.

On the other hand the board will be powered by a battery when "on the field": the shiled has a DCDC converter and I read the battery voltage, so I can just read the bat. voltage and if 0 just assume that I'm powering it through the USB cable and switch to MSD mode...

But I hoped that there was some sort of mechanism integrated in the USB module to automatically detect when the device is connected/disconnected to a host.

Regards Giacomo

0 Kudos
Reply

3,378 Views
ivadorazinova
NXP Employee
NXP Employee

Hi giacomopetrini,

voltage you may to read.

Please, which of these examples do you use? dev_msd_disk_frdmk64f_mqx, dev_msd_disk_frdmk64f_bm ?

Many thanks,

Iva

0 Kudos
Reply

3,378 Views
giacomopetrini
Contributor IV

bare metal.

0 Kudos
Reply

3,378 Views
ivadorazinova
NXP Employee
NXP Employee

Hi,

if you go to disc.c,  you can add the printf if your device is e.g. Attached.

go to void USB_App_Device_Callback(uint8_t event_type, void* val,void* arg)

and add following line 

if(event_type == USB_DEV_EVENT_BUS_RESET)

    {

        g_disk.start_app=FALSE;

    }

    else if(event_type == USB_DEV_EVENT_ENUM_COMPLETE)

    {

        g_disk.start_app=TRUE;

        USB_PRINTF("\n\rAttached\r\n");

    }

and for rejected device (which you must eject by right click on the Removable Disc in Computer)

and add the following line:

switch(event_type)

    {

...

case USB_MSC_START_STOP_EJECT_MEDIA :

            /*  Code to be added by user for starting, stopping or

                ejecting the disk drive. e.g. starting/stopping the motor in

                case of CD/DVD*/

           USB_PRINTF("\n\rRejected\r\n");

            break;

}

now you have an information, when the device was attached and rejected so if you create global variable e.g. unit8_t usb_attached = 0;

and above mentioned fuctions you can change this global variable. In your your logger task you can compare this variable and enable/disable logging.

I hope it helps,

Iva

3,378 Views
giacomopetrini
Contributor IV

OK.

But what I want to do is sense if I need to go to USB mode or normal mode before starting the USB stuff.

I hoped that the USB module in the K60 had some hw flag that is set if a usb cable is connected and reset if the cable is disconneted.

Thanks anyway

Regards Giacomo

PS: it helps anyway, but not for the purpose of my question :smileywink:

0 Kudos
Reply