Problem uninstalling KSDK 1.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem uninstalling KSDK 1.0.0

1,898 Views
cesarrabak
Contributor III

In my chores to upgrade the tool set for Kinetis development I installed KSDK 1.2.0, migrated my important projects and went to the install of KSDK 1.0.0.

However, I got the following message from the uninstaller (first called from the Windows panel, then directly from the folder where it is intalled):

 

49760_49760.jpgKSDK-uninstall.jpg

My platform is Windows 64 bit version 8.1.

 

The Java version is 1.70_25:

Java(TM) SE Runtime Environment (build 1.7.0_25-b17)

Java HotSpot(TM) 64-Bit Server VM (build 23.25-b01, mixed mode)

 

How can I manage to have this uninstall to work?

 

I wouldn't like to have the KSDK_1.0.0 directory tree just deleted as I would start to have dangling entries in the Program Panel of Windows.

 

TIA

--

Cesar Rabak

Labels (1)
0 Kudos
Reply
2 Replies

1,693 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Cesar Rabak,

I tested on my side, Windows 8.1, KSDK 1.0 and Java versions 1.7.0_79-b15, JRE 8 Update 45.

And uninstall was successful.
pastedImage_0.png

ksdk_A.pngksdk_B.png

This error message is very strange because it is typical for Installation, no Uninstall.

If you face the issue during any installation is possible to avoid it by right click on installation icon -> Properties and choose Compatibility

ksdk_.png

Please, try also upgrade your Java versions.

You can also check your Java version here Java Checker

Please, let me know if these tips help you.

I hope it helps you,

Iva

0 Kudos
Reply

1,693 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Cesar,

thank you for you feedback, I´m going to try it and tell you result on my side.

Best Regards,

Iva

0 Kudos
Reply