New Release! Freescale Kinetis SDK version 1.2.0 available now

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

New Release! Freescale Kinetis SDK version 1.2.0 available now

4,892 次查看
mnorman
NXP Employee
NXP Employee

New Release! Freescale Kinetis SDK version 1.2.0 available now

With this new release, we added support for:

     

40 additional Kinetis devices

     

11 more Freescale Freedom boards and Freescale Tower System development boards

     

8 new peripheral drivers

In addition, Kinetis SDK v1.2.0 has:

     

New demos and examples - now organized by evaluation board

     

Added clock manager functionality

     

Simplified clock configuration

     

Optimized example pin mux configuration for low-power

     

Consolidated header, linker and startup files under platform/devices

     

CMSIS-style headers: removed Freescale proprietary style

.

The Kinetis SDK v1.2 continues to include support for FreeRTOS, Micrium® µC/OS -II® and µC/OS–III®, and Freescale MQX RTOS, and it has a growing community of support.

Release Notes

.Download Now

标签 (1)
0 项奖励
回复
4 回复数

4,174 次查看
Rashmitha_Nair
Contributor III

Hi,

I am unable to download the SDK. Is there an alternative link?

 

Regards,

Rashmitha

0 项奖励
回复

4,299 次查看
neilhancock
Contributor IV

Ok - thanks. Yeah the MK21F 120Mhz doesn't have all the features of the MK20D12 - like the 2nd USB HS. and none of the newer devices support the 2nd USB HS with touch that I can see.?

0 项奖励
回复

4,299 次查看
neilhancock
Contributor IV

Just looking at Table 1Addedd device families, which lists  MK20D10 - does that imply the whole MK20D family, so for instance is it MK20D12 - 120Mhz version?

Will certainly try it for the MKL26Z4 that I'm planning on using.

thanks

0 项奖励
回复

4,299 次查看
mnorman
NXP Employee
NXP Employee

The supported devices table uses a shortened form of the part numbers that leaves out the temperature and package codes.  The MK20D10 refers to the 100MHz MK20D devices. Here is the full view of the supported devices in the KSDK_1.2.0\platform\devices folder:

Capture.PNG

The MK21F 120MHz devices are supported but not the older MK20F 120MHz devices.  There is no plan to back-port the KSDK to the devices supported by the TWR-K60F120M eval board.

0 项奖励
回复