Kinetis SDK Project Generator v2 - Windows 10 Support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis SDK Project Generator v2 - Windows 10 Support?

1,711 Views
Deejay
Contributor III

Hi,

I wonder if this is supported on Windows10 platform as I get the following error message:

"This app can't run on your PC. To find a version for your PC, check with the software publisher."

Any idea or work-around solution to run on Windows 10??

Thanks.

 

Regards,

DJ

Labels (1)
0 Kudos
Reply
1 Reply

1,600 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

officially KSDK generator v2 doesn't support win10.

This product has been tested on the following system configurations:

pastedImage_1.png

this information is documented in KSDK Project Generator Release Notes - 2.1.pdf under Kinetis SDK Project Generator v2 folder.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply