Kinetis SDK 1.2.0 Mainline - Linux.gz has wrong extension

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis SDK 1.2.0 Mainline - Linux.gz has wrong extension

1,888件の閲覧回数
720adams
Contributor I

When I download the "Kinetis SDK 1.2.0 Mainline - Linux.gz" file--(sha1 value of 953b103c28fb722631dfbe6593c074a9ed3518b1)  from the community webpage, it is indeed gzipped.  However, it is also a tar file which is not indicated by a simple .gz extension.  Is there some reason the file was not given the .tgz extension?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,659件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Michael,

thank you for your feedback again.

You are right. The extension is not correct. It should indicate it is a tar & gzip archive.

It is fixed for next version.

Please, does it bring you any problem - related to this incorrect extension?

The .tar.gz format should be recognized regardless the extension.

Thank you.

Best Regards,

Iva

0 件の賞賛
返信

1,659件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Michael,

Thank you for the good question.

Please, does it work you all right?

Best Regards,

Iva

0 件の賞賛
返信