Kinetis Bootloader on K21

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Bootloader on K21

4,876 Views
yosigreenbeerg
Contributor I

Hello,

I would like to port "Kinetis Bootloader 2.0" from the K22 example to MK21DN512AVMC5.

 

A according to the documentation the Bootloader project uses KSDK 2.0 drivers and as far as I know,

K21 is not supported by KSDK 2.0 yet.

What steps would you recommend to take in order to perform this port?

 

Thanks,

Yosi.

Labels (1)
0 Kudos
Reply
3 Replies

4,573 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Yosi.

At the moment there is no plan to support MK21DN512AVMC5 in the official KBOOT release yet.

Anyway, you can refer to the guide http://cache.nxp.com/files/soft_dev_tools/doc/ref_manual/KBTLDR200RM.pdf?fpsp=1&WT_TYPE=Reference%20...

where is described Kinetis Bootloader Porting in Chapter 10 and Chapter 11 - Creating a custom flash-resistant bootloader.

I see KSDK support for MK21DN512xxx5.

I hope this helps.

Best Regards,

Iva

0 Kudos
Reply

4,573 Views
ivadorazinova
NXP Employee
NXP Employee

Hello yosi,

I´m gathering information for you. I will answer you as soon as possible.

Thank you for your patience.

Best Regards,

Iva

0 Kudos
Reply

4,572 Views
yosigreenbeerg
Contributor I

Hello Iva,

Thank you for your message, I will wait for your answer.

Best regards,

Yosi.

0 Kudos
Reply