KSDK Project Generator v2.3 Available Now

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KSDK Project Generator v2.3 Available Now

4,057 Views
mnorman
NXP Employee
NXP Employee

The KSDK Project Generator Tool V2.3 is available on NXP web page. Click here to go to the download web page. You can find the download link under the “Initialization/Boot/Device Driver Code Generation”.

 

1. What’s new in V2.3:
Support generation of standalone cloned project – updated for IAR EWARM and KEIL MDK to fix several issues

 

2. Features:
The following features are available with the KSDK Project Generator tool:

 

  • Cross platform
    • Operates on Windows, Linux, and Mac OSX
    • Developed in 32-bit Python 2.7 on Windows 7, Ubuntu 14.10, OSX 10.10 & 10.11
  • Supports KSDK 1.2.0, 1.3.0 and 2.x
  • Quick Generate of development board based KSDK projects
  • Advanced Generate of New KSDK based projects
    • Device or development board based
    • Linked to KSDK installation or standalone
    • RTOS support ( when project with FreeRTOS is created part of source code is licensed with GPL-2.0 WITH the
    • FreeRTOS GPL exception license)
    • HAL or Platform library level projects (for KSDK 1.2, 1.3)
    • Libraries in standalone projects tailored to device package (for KSDK 1.2, 1.3)
    • KDS, IAR, Keil MDK, and/or Atollic TrueSTUDIO IDE projects
    • Generation of standalone or linked cloned project

 

3. Please refer to the release notes (attached) for more details

Labels (1)
0 Kudos
Reply
1 Reply

3,375 Views
kelliott
Contributor I

The release notes imply that there's support for IAR included. When I run the tool in Advance mode, the only available tool is the Kinetis Design Studio. How do I generate a project for IAR?

0 Kudos
Reply