KSDK_1.3.0 DSPI issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KSDK_1.3.0 DSPI issue

1,440 Views
carlossilva
Contributor I

Hello, im using SPI and the fsl_dspi official driver, I noticed that when I used DSPI_MasterTransferBlocking function, i got an unhandled interrupt .

 

Here is my setup: KSDK_1.3.0 board: frdmk64f.

Labels (1)
0 Kudos
Reply
1 Reply

1,360 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Carlos,

After the unhandled interrupt occurs, pls check the interrupt source index in the xpsr in debugger of the tools you are using, the bit0~8 of xpsr register represent the interrupt source index.

If the interrupt source index is 3(hard fault interrupt), it is a bit complicated, for example you use a peripheral whose clock is not enabled, or you access a memory which does not exist, all of the case can lead to hardware fault interrupt.

Anyway, i suggest you download SDK2.0 package from the link:

http://www.nxp.com/ksdk

Hope it can help you

BR

Xiangjun Rong

0 Kudos
Reply