K40D & KSDK 2.0 examples

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K40D & KSDK 2.0 examples

1,207 Views
Eric_t
Contributor III

Hi,

 

I am going to use MK40DX256VMD10 controller with KSDK 2.0 and KDS 3.2

I have bought the TWR-K40D100M and I tried to generate examples with the SDK builder.

The problem is that even if I choose the MK40DX256VMD10 , the SDK builder generates examples for K60 controller.

So, I suppose that K40 and K60 are full compatible and the only thing I have to do is to change processor from K60 to MK40DX256VMD10. 

Unfortunately every attempt to change the processor leads to compile errors.

Does anyone know how can I do it?

 

Thank you     

Labels (1)
0 Kudos
Reply
1 Reply

1,088 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

 I downloaded the SDK2.0 driver previously based on K40, the example was based on MK60D10, but there were  driver for both K40 and K60.

Pls refer to the directory:

for K40 driver, pls go to the directory.

C:\Freescale\SDK2.0_PROCESSOR_K40\devices\MK40D10\drivers

for K60 driver, pls go to the location:

C:\Freescale\SDK2.0_PROCESSOR_K40\devices\MK60D10\drivers

BR

Xiangjun Rong

0 Kudos
Reply