I need a FreeRTOS Reference Manual for v8.2.3.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I need a FreeRTOS Reference Manual for v8.2.3.

2,391 Views
rogerchaplin
Contributor II

I'm starting development on a new project with KSDK 2.0, used the KSDK builder to create the SDK download. It comes with FreeRTOS v8.2.3 bundled. However, on the FreeRTOS website the only documentation I can find is for v9.0.0 which has some significant changes. Did somebody at Freescale/NXP tuck away a copy of the v8.2.3 reference manual they'd be willing to share? And knowing the tendency of Real Time Engineers, Ltd. to hide away old versions of documentation, wouldn't it make sense to bundle the correct version of the FreeRTOS reference manual along with the "Getting Started with KSDK and FreeRTOS OS" document when you build the KSDK for download?

Tags (2)
0 Kudos
Reply
1 Reply

1,967 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Roger,

It seems that you can download the version 8.2 of FreeRTOS RM from the link:

http://www.freertos.org/Documentation/FreeRTOS-Reference-Manual-Table-of-Contents.pdf 

Pls have a try

BR

Xiangjun Rong

0 Kudos
Reply