How to use freescale k64f  flexbus ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use freescale k64f  flexbus ?

2,948件の閲覧回数
zhailing
Contributor II

Hi

    Now I want to use flexbus to config the fpga; i can't find design demo of flexbus;only the driver 

flexbus_config_t flexbusConfig;
FLEXBUS_GetDefaultConfig(&flexbusConfig);
flexbusConfig.waitStates = 2U;
flexbusConfig.chipBaseAddress = 0x60000000U;
flexbusConfig.chipBaseAddressMask = 7U;
FLEXBUS_Init(FB, &flexbusConfig);

I  use the demo config the flexbus;but i can't measure

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,693件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, ZhaiLing,

As you said that we have not the example code for FlexBus. The FlexBus configuration is only dependent on your hardware connection, for example, the port size, wait state, byte-lane shift, multiplexed or non-multiplexed mode...

Anyway, the flexbusConfig structure corresponds to the FlexBus register contents, pls refer to the Chapter 31
External Bus Interface (FlexBus) in RM of K64, especially register setting.

After the FlexBus register setting, you can use a pointer to access the external memory, which locates in the FlexBus memory space, pls refer to Chapter 4 Memory Map.

If you still have question, pls tell us the hardware connection so that we can determine the flexbus register setting.

BR

Xiangjun Rong

0 件の賞賛
返信

2,693件の閲覧回数
zhailing
Contributor II

hi,xiangjun.rong

  I read the date from the fpga;the flexbus  address is 0x8003,the date is 0x77.

But i read the date is 0x17.I don't kown why ? where is the 0x17 come from?  

The _51RDLVT is FB_OE.

     pastedImage_1.png

Thanks and best regards

zhai

0 件の賞賛
返信

2,693件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, ZhaiLing,

Does the timing is from logic analyzer or tools of FPGA, I think it is possible that the data become from 0x77 to 0x17, when  the FB_OE becomes high, which means that the FPGA do not drive the data bus, in other words, the data bus is float when  the FB_OE becomes high.

BR

Xiangjun Rong

0 件の賞賛
返信

2,693件の閲覧回数
zhailing
Contributor II

Hi xiangjun.rong

  Yes,I grab the signal with the signaltap ii; The date of  fpga send is always 0x77;when  the FB_OE becomes high ,the date shoud be 0x77;

pastedImage_1.png

my configrations

void FLEXBUS_GetDefaultConfig(flexbus_config_t *config)
{
config->chip = 0; /* Chip 0 FlexBus for validation */
config->writeProtect = 0; /* Write accesses are allowed */
config->burstWrite = 0; /* Burst-Write disable */
config->burstRead = 0; /* Burst-Read disable */
config->byteEnableMode = 0; /* Byte-Enable mode is asserted for data write only */
config->autoAcknowledge = true; /* Auto-Acknowledge enable */
config->extendTransferAddress = 0; /* Extend transfer start/extend address latch disable */
config->secondaryWaitStates = 0; /* Secondary wait state disable */
config->byteLaneShift =kFLEXBUS_Shifted;//kFLEXBUS_NotShifted; /* Byte-Lane shift disable */
config->writeAddressHold = kFLEXBUS_Hold1Cycle; /* Write address hold 1 cycles */
config->readAddressHold = kFLEXBUS_Hold2Or1Cycles; /* Read address hold 0 cycles */
config->addressSetup =
kFLEXBUS_FirstRisingEdge; /* Assert ~FB_CSn on the first rising clock edge after the address is asserted */
config->portSize = kFLEXBUS_1Byte; /* 1 byte port size of transfer */
config->group1MultiplexControl = kFLEXBUS_MultiplexGroup1_FB_ALE; /* FB_ALE */
config->group2MultiplexControl = kFLEXBUS_MultiplexGroup2_FB_CS4; /* FB_CS4 */
config->group3MultiplexControl = kFLEXBUS_MultiplexGroup3_FB_CS5; /* FB_CS5 */
config->group4MultiplexControl = kFLEXBUS_MultiplexGroup4_FB_TBST; /* FB_TBST */
config->group5MultiplexControl = kFLEXBUS_MultiplexGroup5_FB_TA; /* FB_TA */
}

The minmum time of FB5 shuld be  0.5 ns.Is it the reasion to make it? How to adujst it?

Thanks and best regards!

zhai

0 件の賞賛
返信