How do I get support for the MLK05?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I get support for the MLK05?

1,203件の閲覧回数
davidzeichner
Contributor I

I'm looking for mainline support (Not ProcessorExpert) for the KL05 processor. KSDK 1.1.0 & 1.3.0 don't seem to have it? Is there any toolkit that does?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,080件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello David,

Yes , as so far , the KSDk do not support the KL05,

except the Processor Expert , there is a driver lib on the wibsite :

FRDM-KL05Z Sample Code Package

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信