Hi Erich and Daniel,
Thanks for your answer. I couldn´t answer you before because I’m busy with a develop. I know what you say but I haven´t found in MCUxpresso for my MK20dx256vlh7 microcontroller that I’m working in this moment. Do you know if there are SDKs for this microcontroller.
Anyway I have found one way to start a new project from another existing project with a different name following some simple steps that maybe you know.
These steps are: Go to the main project folder, click right in this folder and select “Rename”.
Not only this basic step.
Then go to “Project” option and select “Properties”, in the left side of the window that is open select C/C++ Build, and select “Settings”, go to “Buld Artifact” and select “$” in Artifact Name.
Then go to “Project” option and select “Clean”, a window appears like bellow and select OK with the shown options.
In Debug configuration select the next that I show you:
and change the name of the project in main tab of Debug Configurations Window in the places that I show you in the red rectangles.
The last step is to remove all files that there are remaining with old names in Debug, Project Settings/Linker files folders from the project and we don’t need them. Select them and click right and select “Delete”.
I don’t know if there is any more simple way but I do it this way and for me it works.
I hope it’s useful for your help.
Regards,
Arturo Arteaga,
De: BlackNight
Enviado el: miércoles, 05 de abril de 2017 10:02
Para: Arturo Arteaga
Asunto: Re: - Re: How can I start a new project from another existing project with a different name?
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community
Re: How can I start a new project from another existing project with a different name?
reply from Erich Styger <https://community.nxp.com/people/BlackNight?et=watches.email.thread> in Kinetis Software Development Kit - View the full discussion <https://community.nxp.com/message/893954?commentID=893954&et=watches.email.thread#comment-893954>