How can I start a new project from another existing project with a different name?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I start a new project from another existing project with a different name?

10,853件の閲覧回数
arturoarteaga
Contributor II

Hi,

I want to begin a new project from another existing project, but I don't want to keep the previous name of original name.

How can I rename the new project?? I have tried but when I compile it, Ihave some errors in Debug carpet in "makefile" file.

Thanks in advanced,

Regards,

Arturo Arteaga

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

10,327件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Arturo,

I recommend that you have a look at the NXP MCUXpresso IDE, see MCUXpresso IDE: Unified Eclipse IDE for NXPs ARM Cortex-M Microcontrollers | MCU on Eclipse  and especially the 'New Project' section. What the NXP MCUXpresso IDE has is the ability to import/clone an existing SDK example project with a new name:

Use the Import function:

pastedImage_2.png

Select the Board/SDK:

pastedImage_3.png

Then select the projec(s) and give it a name:

pastedImage_4.png

This then clones an existing SDK project under a new name.

I hope this helps,

Erich

0 件の賞賛
返信

10,322件の閲覧回数
arturoarteaga
Contributor II

Hi Erich and Daniel,

Thanks for your answer. I couldn´t answer you before because I’m busy with a develop. I know what you say but I haven´t found in MCUxpresso for my MK20dx256vlh7 microcontroller that I’m working in this moment. Do you know if there are SDKs for this microcontroller.

Anyway I have found one way to start a new project from another existing project with a different name following some simple steps that maybe you know.

These steps are: Go to the main project folder, click right in this folder and select “Rename”.

Not only this basic step.

Then go to “Project” option and select “Properties”, in the left side of the window that is open select C/C++ Build, and select “Settings”, go to “Buld Artifact” and select “$” in Artifact Name.

Then go to “Project” option and select “Clean”, a window appears like bellow and select OK with the shown options.

In Debug configuration select the next that I show you:

and change the name of the project in main tab of Debug Configurations Window in the places that I show you in the red rectangles.

The last step is to remove all files that there are remaining with old names in Debug, Project Settings/Linker files folders from the project and we don’t need them. Select them and click right and select “Delete”.

I don’t know if there is any more simple way but I do it this way and for me it works.

I hope it’s useful for your help.

Regards,

Arturo Arteaga,

De: BlackNight

Enviado el: miércoles, 05 de abril de 2017 10:02

Para: Arturo Arteaga

Asunto: Re: - Re: How can I start a new project from another existing project with a different name?

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community

Re: How can I start a new project from another existing project with a different name?

reply from Erich Styger <https://community.nxp.com/people/BlackNight?et=watches.email.thread> in Kinetis Software Development Kit - View the full discussion <https://community.nxp.com/message/893954?commentID=893954&et=watches.email.thread#comment-893954>

0 件の賞賛
返信

10,322件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Arturo:

I would suggest you use  the tool --KSDK Code Generator , You only need to provide a valid KSDK installation path, enter a name for your new project, and select a board from the list of boards.   Please refer to the below link.

New Kinetis SDK Project Generator v2 is available! 

You can download this tool from

http://www.nxp.com/products/wireless-connectivity/2.4-ghz-wireless-solutions/ieee-802.15.4-plus-ble/...

Regards

Daniel

0 件の賞賛
返信