Enabling collaboration on KSDK Device Drivers in github

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enabling collaboration on KSDK Device Drivers in github

1,069件の閲覧回数
maxv
Contributor I

Is there any chance NXP would consider allowing for more collaborative development of device drivers and SDK code in github?

 

 

It seems like it would be a benefit to anyone working on Kinetis or LPC devices to have faster access to upstream code changes via a platform like Github, and any helpful modifications would also be easier to pull back in from the community...

 

I mention this because of another question I just asked, in which case it would be pretty easy to create a pull request for changes I could make that would benefit others.

 

One can also see the benefits of this model working for the rapidly-evolving mbed platform.

ラベル(1)
0 件の賞賛
返信
0 返答(返信)