ECC with SD card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ECC with SD card

1,791 Views
PO220
Contributor IV

Hi

 

I'm using kinetis (K27 or K64) with SD card and FatFs, ok, no problem;

I try to understand where the ECC is managed : The nand flash technology is not reliable, we must handle the errors with ECC.

Is ECC managed by the hardware controller in the sd card or is it the SDK and the filesystem that do the ECC correction ?

I thought it was in the card but the SD card builders do not talk about ECC in documentations...

 

Thank you in advance.

Labels (1)
0 Kudos
Reply
2 Replies

1,554 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi PO220,

From what I saw on the projects, the only places where the ECC is referenced is in the KSDK libraries.

I think that the SDK takes care of the ECC instead of the SD. 

let me investigate more about this and I will tell you.

Sorry for the  delay and late response.

have a great day.

Best regards.

Jonathan

0 Kudos
Reply

1,554 Views
PO220
Contributor IV

Thanks

0 Kudos
Reply