ECC with SD card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ECC with SD card

1,775件の閲覧回数
PO220
Contributor IV

Hi

 

I'm using kinetis (K27 or K64) with SD card and FatFs, ok, no problem;

I try to understand where the ECC is managed : The nand flash technology is not reliable, we must handle the errors with ECC.

Is ECC managed by the hardware controller in the sd card or is it the SDK and the filesystem that do the ECC correction ?

I thought it was in the card but the SD card builders do not talk about ECC in documentations...

 

Thank you in advance.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,538件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi PO220,

From what I saw on the projects, the only places where the ECC is referenced is in the KSDK libraries.

I think that the SDK takes care of the ECC instead of the SD. 

let me investigate more about this and I will tell you.

Sorry for the  delay and late response.

have a great day.

Best regards.

Jonathan

0 件の賞賛
返信

1,538件の閲覧回数
PO220
Contributor IV

Thanks

0 件の賞賛
返信