Does KSDK 1.2.0 have processor expert support for the TWR-K21F120M to operate as a USB host for MSD class?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does KSDK 1.2.0 have processor expert support for the TWR-K21F120M to operate as a USB host for MSD class?

1,299 Views
kevinpenn
Contributor I

I see a PE component for fsl_usb_device_msd_class but nothing for host.  My goal is to have the board have the ability to update its firmware when a USB stick is attached containing new firmware. I believe I am right in thinking that the board would need to be a host for MSD.  Any insight or information how I can accomplish this?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,186 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Kevin,

I am  sorry, but the PEx in KDS 3.0 doesn't support Host mode, and for  device, only HID and MSD class are supported. You may refer  to page 13 of KSDK_1.2.0_Eclipse_Update_Release_Notes.pdf(C:\Freescale\KDS_3.0.0\eclipse\ProcessorExpert)  for more details.

so maybe you have to use the source code directly in your project.


Have a great day,
Kan

Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply