D Current Scaling Not 1:1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

D Current Scaling Not 1:1

4,922件の閲覧回数
derekcook
Senior Contributor I

Hello, 

I am applying D current to my motor while running in speed mode to artificially load down my system to validate system functionality at high current. If I set the D current reference - tempStatorRefCurrentDQ.d to 150A, I get 50A of current on my A, B and C phases. What causes this scale factor? Why is the D current reference not instead adding 150A of current on my A, B and C phases? 

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

4,759件の閲覧回数
linestream-adam
Senior Contributor I

Derek,

When you modify the D axis reference, you are adding magnetic flux into the motor. This will change the response of the motor to Q axis current. Without monitoring both values, it is difficult to determine what the current value should be. Is the 50A you are measuring the peak value or rms value?

0 件の賞賛
返信

4,759件の閲覧回数
derekcook
Senior Contributor I

Adam, what would be the formula to determine how much current injecting D current (flux) should add to my system?

0 件の賞賛
返信

4,759件の閲覧回数
derekcook
Senior Contributor I

Hey Adam, 

I am aware I am adding magnetic flux to the motor. I just was wanting to know if there is any way to determine the amount of current injecting the magnetic flux will add to my system? I am monitoring RMS ABC current. 

0 件の賞賛
返信

4,759件の閲覧回数
derekcook
Senior Contributor I

Hey Adam, 

Is there a way to determine the amount of current injecting magnetic flux will add to my system? What is this equation?

0 件の賞賛
返信