xPico Wi-Fi with K70 tower

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

xPico Wi-Fi with K70 tower

1,680 Views
dongyangli
Contributor I

I wonder if xPico Wi-Fi compactable with K70 tower? If so, is there any demo available?

0 Kudos
Reply
2 Replies

1,570 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

TWR-LTRX-XPWK: xPico® Wi-Fi® Tower System Peripheral Module provided by Lantronix, which is compatible with the Freescale Tower System.

Please contact with Freescale Third Partner Lantronix for the detailed info.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,570 Views
dongyangli
Contributor I

Thank you so much, I will check it out.

Quoting Hui_Ma <[email protected]>:

Hui_Ma

replied to the discussion

"xPico Wi-Fi with K70 tower"

To view the discussion, visit:

https://community.freescale.com/message/567977?et=watches.email.thread#567977

>

0 Kudos
Reply