while flashing i got this error "{Error in services launch sequence}" plz give sollution to solve this

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

while flashing i got this error "{Error in services launch sequence}" plz give sollution to solve this

6,247件の閲覧回数
gobis
Contributor I

pastedImage_1.png

0 件の賞賛
返信
7 返答(返信)

6,019件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi gobi s

This error occurs when you are no selecting you interface correctly, Could you explain you case more:

Debug configuration?

What example code are you using?

MCU that you are using?

Regards

Jorge Alcala

0 件の賞賛
返信

6,019件の閲覧回数
gobis
Contributor I

Hi Jorge,

Thanks for your reply...sorry for late reply,,

Details below about your questions..

Debug configuration?

GDB PEMicro Interface debugging

MCU that you are using?

Our freescale controller is MKE02Z64 VQH4(MODEL: FDRM-KE02740M)..into

controller MKE02Z16VLC4 I want to flash.

What example code are you using?

Actually i am using the code which already developed by some one...no

error in that because who developed that code they had flashed &

checked..in my end it is not happening...i need your support to finish

that flashing..

Thanks

S.Gobi

0 件の賞賛
返信

6,019件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi gobi s

Could you share a screenshot of your debug configuration? in P&E micro it should appear selected an Interface and a PORT in the debug configuration window as follow in the next image:

pastedImage_1.png

If you are not able to select both of them, please check that your device manager can identify your debug interface and let me know what you get.

Hope this helps,

Best Regards

Jorge Alcala

0 件の賞賛
返信

6,019件の閲覧回数
gobis
Contributor I

Hi jorge,

In device manager it is OpenSDA- CDC Serial port(com7) comes

underports(com&lpt).

thank you

0 件の賞賛
返信

6,019件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

a common reason for that "error in services launch sequence" message is that there is a dangling GDB server. See https://mcuoneclipse.com/2015/05/18/gdb-client-and-server-unlocking-gdb/ . Can you check that the P&E GDB server is not still running (if so, kill it in the task manager)?

I hope this helps,

Erich

0 件の賞賛
返信

6,019件の閲覧回数
gobis
Contributor I

thanks eric..for your support

I found problem, and I had flashed...

problem is firmware of freescale board is not updated..

0 件の賞賛
返信

6,019件の閲覧回数
gobis
Contributor I

Hi jorge,

plz find the attachment of screenshot of my debug configuration..as you said

port i cant able to select but in device manager, i checked driver for

freescale got installed . Eventhough i cant select port..

Thank you

Jorge Antonio Alcala Vazquez

replied to the discussion

"Re: while flashing i got this error "{Error in services launch sequence}"

plz give sollution to solve this"

To view the discussion, visit:

https://community.nxp.com/message/839432?commentID=839432&et=watches.email.thread#comment-839432

>

0 件の賞賛
返信