what's the link between LCD waveform registers and LPUART.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what's the link between LCD waveform registers and LPUART.

1,157 Views
Avinash_7
Contributor I

Hi,

I am working on MKM34Z256xxx7, it is connected to 32pin segment LCD and LPUART for communication purpose(both are working fine).

I run the controller in VLPR and VLPS modes by switching for every 1 second. I'm using LCD on PORTA, PORTB, PORTC, PORTD and LPUART on PORTI. The issue is, if I turn on all LCD segments by will filling (0xFF) in respective waveform registers and try to send some data on LPUART, I could able to receive only a few bytes on interrupt, not getting interrupt for rest of other bytes. The LPUART interrupts are not working. If I turn off a any single segment by writing (0x00) on LCD waveform registers, then my data goes normally on LPUART.

I verified clock initializations, interrupt enable/disable stuff, respective voltages on LPUART rx/tx pins, waveforms and controller switch to VLPR whenever it get tx/rx/edge interrupts  as well. I also found that if I keeps running in VLPR state, then everything working fine as expected. I was been working on this from past 3 days.

Please help me to crack this strange issue I'm facing. Thanks in advance.

Regards,

Avinash.

0 Kudos
Reply
1 Reply

1,095 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @Avinash_7 ,

How is the problem going? Please check the NVIC->IPCR register to see if the interrupt is pending and check NVIC->ISER register to see if LPUART interrupt is enabled at that time.

 

Regards,

Jing

0 Kudos
Reply