twr km34z emeter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

twr km34z emeter

2,277 Views
venkatkrishna
Contributor II

Hi,

         I recently purchased TWR-KM34Z50.

I am trying the energy meter demo project using codewarrior 10.6 and freemaster 2.0.

While runningthe project,  Frequency in the LCD shows only 24.880hz(freemaster setting 50Hz).

I tried by changing the frequency variable in FreeMaster from 45 to 65.5.But the LCD display

shows always close 49% of setting value.Voltage is 274.25 Volts Current is 27.668Amps.

Did i missed anything.

Please help to solve the issue.

Please tell me the accuracy of K20 generator ouput .

Thanks/regards,

K.Venkat

Labels (1)
0 Kudos
Reply
2 Replies

1,654 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Venkat,

Regarding your question, first of all, pls check the simulated 3phase voltage/current signal frequency, I suggest you connect the signal pin1 of J17 to oscilloscope and check the voltage frequency on scope. I suppose the G20 generates the correct frequency signal.

I have the TWR-KM34Z50 board, but the measurement code has been rewritten by somebody, can you attach the measurement code based on KM34 so that I can test it on my board? or you can give me a link to download it.

BR

Xiangjun Rong

0 Kudos
Reply

1,654 Views
venkatkrishna
Contributor II

Hi Xiangjun Rong,                           Thank you for reply.I didn't tested the output signal so far.Soon i will test it with OSCILLOSCOPE.I used the code downloaded from the website.If i run the project,it displayedFrequncy less then the set value in freemaster(49% of the setvalue).Please find the demo code at http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/kinetis-cortex-m-mcus/m-series/kinetis-m-series-tower-system-module:TWR-KM34Z50M?fpsp=1&tab=Design_Tools_Tab

I want to confirm the accuracy of the code generator.Please help me. Thanks/Regards,

K.VENKATAVARADHAN.

From: xiangjun.rong <[email protected]>

To: Venkat Krishna <[email protected]>

Sent: Monday, 23 May 2016 1:40 PM

Subject: Re: - twr km34z emeter

#yiv6550155019 * #yiv6550155019 a #yiv6550155019 body {font-family:Helvetica, Arial, sans-serif;}#yiv6550155019 #yiv6550155019 h1, #yiv6550155019 h2, #yiv6550155019 h3, #yiv6550155019 h4, #yiv6550155019 h5, #yiv6550155019 h6, #yiv6550155019 p, #yiv6550155019 hr {}#yiv6550155019 .yiv6550155019button td {}

|

NXP Community

|

twr km34z emeter

reply from xiangjun.rong in Kinetis Microcontrollers - View the full discussionHi, Venkat, Regarding your question, first of all, pls check the simulated 3phase voltage/current signal frequency, I suggest you connect the signal pin1 of J17 to oscilloscope and check the voltage frequency on scope. I suppose the G20 generates the correct frequency signal.I have the TWR-KM34Z50 board, but the measurement code has been rewritten by somebody, can you attach the measurement code based on KM34 so that I can test it on my board? or you can give me a link to download it.BRXiangjun Rong

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in Kinetis Microcontrollers by email or at NXP Community

Following twr km34z emeter in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences |

|

0 Kudos
Reply