when i try to connect the twr k70 with the terminal utlity i can not open the port and i read "Failed to Open. Plug DEMO board into PC via USB cable" even if with another program that putty i open the com.
another problem is that the osbdm is not recognized as a usb com but as a generic com.
i try to follow the troubleshooting guide from pemicro site but nothing...
can anyone help me?
Hello ,
"t the osbdm is not recognized" , so does your project have been download to the board?
Please check the J10 on board, do not connect the pin 1 and 2 of J10.
Then the normal situation is like this :
Hope it helps
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
Osbdm is normally recgonized buti f i check in computer i dont see the peripheral. Is normal?
If I create an exe how to load this file in the tower?
thanks
Da: Alice_Yang
Inviato: lunedì, 7. marzo 2016 10:43
A: Francesco Gerardi <gerardi@orchestraweb.com>
Oggetto: Re: - twr-k70--> Failed to Open. Plug DEMO board into PC via USB cable
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community
twr-k70--> Failed to Open. Plug DEMO board into PC via USB cable
reply from Alice_Yang <https://community.freescale.com/people/Alice_Yang?et=watches.email.thread> in Kinetis Microcontrollers - View the full discussion <https://community.freescale.com/message/622012?et=watches.email.thread#comment-622012>
Hi Francesco,
- Although you can not find it in the computer management , how do you know
"Osbdm is normally recgonized" ?
- About how to download the project to board , please refer to the screenshot :
if the board is recognized , it will show in the Port :
then click "Debug", if it show update the firmware, please refer to the reminder to operate ,
in teh TWR-K70 board , the bootloader header is J10:
click OK, when it start update ,you can see
After the update , you can download it now .
If still have problem on your side ,please also take a screenshot about it , then we can solve
it sooner .
Hope it helps
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
I have another question for you :smileyhappy:
I have download egui demo and I would upload this in the twr-k70 .
Which program I have need to do this? I can upload this only with the usb ?
thanks
Da: Alice_Yang
Inviato: mercoledì, 16. marzo 2016 09:52
A: Francesco Gerardi <gerardi@orchestraweb.com>
Oggetto: Re: - twr-k70--> Failed to Open. Plug DEMO board into PC via USB cable
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community
twr-k70--> Failed to Open. Plug DEMO board into PC via USB cable
reply from Alice_Yang <https://community.freescale.com/people/Alice_Yang?et=watches.email.thread> in Kinetis Microcontrollers - View the full discussion <https://community.freescale.com/message/625304?et=watches.email.thread#comment-625304>
HI,
You can also use some other debuggers , for example P&E multilink .
Alice