stop mode with RTC or any timer interrupt.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

stop mode with RTC or any timer interrupt.

1,548件の閲覧回数
cesarpavlak
Contributor I
Hello, I need to put the mk22fn512 in stop mode by using the KDS . 

to wake-up would like to use the internal RTC to monitor keyboard and alarms. 

any suggestions of how to do this ?.

 Grateful
1 返信

1,437件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The following give details about RTC and using it as LLWU wake up source:
http://www.utasker.com/kinetis/LLWU.html
http://www.utasker.com/kinetis/KL_RTC.html

There are operational references at:
http://www.utasker.com/kinetis/FRDM-K22F.html
http://www.utasker.com/kinetis/TWR-K22F120M.html
http://www.utasker.com/kinetis/BLAZE_K22.html
if you want to see it in action.

Built with KDS.

Regards

Mark

Kinetis for professionals: http://http://www.utasker.com/kinetis.html