startup kit needed for TWR-KL25Z48M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

startup kit needed for TWR-KL25Z48M

1,969件の閲覧回数
huishao2
Contributor IV

Hi-

I got a TWR-KL25Z48M demo board with Atheros WiFi board mounted underneath. My development GUI is IAR. When I plug in USB cable to the board, my PC shows "unrecognized device".


Someone suggests me to use PEMICRO from IAR to debug the board, but I can't connect it successfully.

Can someone point me to the documents/startup kit/demo project to enable the TWR board? I need it to test communications with WiFi AP.

Thanks!

Hui

0 件の賞賛
返信
4 返答(返信)

1,799件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Have you programmed the debugger to the board?

It should show up as a hard drive and on the hard drive there is a link to the P&E web site with instructions and latest drivers.

I have attached the FRDM-KL25 one that I use.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html

KL25: http://www.utasker.com/kinetis/FRDM-KL25Z.html / http://www.utasker.com/kinetis/TWR-KL25Z48M.html

For the complete "out-of-the-box" Kinetis experience and faster time to market

:smileyinfo: Out-of-the-box support for 46 Kinetis boards and 10 IDEs (460 combinations from a single code source with no porting required)

0 件の賞賛
返信

1,799件の閲覧回数
huishao2
Contributor IV

Hi Mark,

I believe this TWR board was used by someone else already. So the debugger should be in place. However, when I plug in USB to PC, it doesn't show as a harddrive.

Just now I tried plugging USB while pressing reset button, PC shows "installing openSDA application..." and Device Mangers shows a PEmicro CDC device for a short while. Then everything is gone. USB device still has a question mark on it.

thanks!

Hui

0 件の賞賛
返信

1,799件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

I am a little confused on what you metioned " use PEMICRO from IAR to debug the board". What you really used as the debugger?

0 件の賞賛
返信

1,799件の閲覧回数
huishao2
Contributor IV

Hi Fang

In IAR GUI, there is Project->Options->Debugger->Driver->PE micro, which is one of the debugging measures supported by IAR.

I am talking about this is because the JTAG is built in on TWR board so I don't need I-jet to load/debug code onto the board. Instead, I can just use a USB cable to do all kinds of those things.

Problem here is I have the TWR board, but nobody can recall how it was brought up, like what PC drivers are needed, how to download code and debug it etc, since it has been long time.

Looking forward to your advise.

Thanks!

Hui

0 件の賞賛
返信