size of *.elf file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

size of *.elf file

1,335 次查看
roymessinger
Contributor V

How do I know if the size of my code to flash will be sufficient for my SRAM size of the controller?

Where can I look for the my code flash size?

0 项奖励
回复
3 回复数

1,177 次查看
BlackNight
NXP Employee
NXP Employee

Hi Roy,

that depends on the toolchain used. I assume you are using gcc and Kinetis Design Studio, then you can turn on the size informatio:

pastedImage_4.png

See Code Size Information with gcc for ARM/Kinetis | MCU on Eclipse  for details about this.

This will report you the size in the console view after linking. This is usin the 'size' utility (see that post) which gives you all kind of information.

text, data and bss: Code and Data Size Explained | MCU on Eclipse  explains the meaning of the information printed.

Another way would be to look at the linker .map file.

I hope this helps,

Erich

0 项奖励
回复

1,177 次查看
roymessinger
Contributor V

Ok, thank you.

Where do I look at the .map file?

I've tried looking there but it's a very large file...

Roy

0 项奖励
回复

1,177 次查看
BlackNight
NXP Employee
NXP Employee

Hi Roy,

yes, that's correct, there is no single place in the GNU Linker map file to look at. You get all the details, but no summary. You need to use the size tool as outlined by these articles if you want a summary.

Erich

0 项奖励
回复