size of *.elf file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

size of *.elf file

1,837件の閲覧回数
roymessinger
Contributor V

How do I know if the size of my code to flash will be sufficient for my SRAM size of the controller?

Where can I look for the my code flash size?

0 件の賞賛
返信
3 返答(返信)

1,679件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Roy,

that depends on the toolchain used. I assume you are using gcc and Kinetis Design Studio, then you can turn on the size informatio:

pastedImage_4.png

See Code Size Information with gcc for ARM/Kinetis | MCU on Eclipse  for details about this.

This will report you the size in the console view after linking. This is usin the 'size' utility (see that post) which gives you all kind of information.

text, data and bss: Code and Data Size Explained | MCU on Eclipse  explains the meaning of the information printed.

Another way would be to look at the linker .map file.

I hope this helps,

Erich

0 件の賞賛
返信

1,679件の閲覧回数
roymessinger
Contributor V

Ok, thank you.

Where do I look at the .map file?

I've tried looking there but it's a very large file...

Roy

0 件の賞賛
返信

1,679件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Roy,

yes, that's correct, there is no single place in the GNU Linker map file to look at. You get all the details, but no summary. You need to use the size tool as outlined by these articles if you want a summary.

Erich

0 件の賞賛
返信