problem with kinetis_sc lcdc example on twr-k70f120m

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

problem with kinetis_sc lcdc example on twr-k70f120m

跳至解决方案
4,147 次查看
claudiomechini
Contributor II

Good morning, My name is Claudio Mechini and I am a software developer of the LED SpA company. We have to evaluate the LCDC controller features of the kinetis K70 so we have bought the tower system TWR-K70F120M with TWR-SER module and TWR-LCD-RGB module. With this configuration I had flashed the micrcocontroller with your LCDC demo example (and also lcdc_rev2) of the package "KINETIS SC" but I have a problem. When the demo start the display of the twr-lcd-rgb show for just a second the correct windows composed by four square of different color,red,green,blue and white and a center rectangle with black colour (IM008804.jpg), and then show other windows with rows and columns of random colours like the clock is absent(IM008805.jpg and IM008806.jpg) , but all the signals, hsync,vsync,clk,de, are present, I have controlled them with digital scope. So what is the cause? I have tried also with lcdc-rev2 demo but there is the same issue. I hope that you can help me. Thanks you. Best regards

标签 (1)
0 项奖励
回复
1 解答
3,873 次查看
LuisCasado
NXP Employee
NXP Employee

Hello Claudio,

Please try to change the lcdc.c file in your project for the attached. That configuration is working in all the TWR-LCD-RGB revisions.

Best Regards,

Luis

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,874 次查看
LuisCasado
NXP Employee
NXP Employee

Hello Claudio,

Please try to change the lcdc.c file in your project for the attached. That configuration is working in all the TWR-LCD-RGB revisions.

Best Regards,

Luis

0 项奖励
回复
3,873 次查看
claudiomechini
Contributor II

Thank you very very much Luis. Now can I go to the next step. Have a nice day. Best regards. Claudio

0 项奖励
回复