measure time using FTM input capture

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

measure time using FTM input capture

1,561 Views
rodolfocazares
Contributor I

I am using micro kinetis MKE02Z64VLC4  to measure time trougth FTM input capture. Project was initied on process expert.

I need to reset counter in each event and I call 

** ===================================================================
** Method : EncoderA_Reset (component Capture)
** Description :
** This method resets the counter register (see implementation
** note in <General Info>).

But counter is not reset.

Where I can see how I need implement it ??

0 Kudos
Reply
1 Reply

1,224 Views
egoodii
Senior Contributor III

You don't describe exactly what *kind* of time you are measuring, but in any case it is FAR better NOT to reset the counter during operation, as you will most likely run into race conditions and/or inconsistent measurements.  Let the counter free-run (modulo 65536) and simply use unsigned 16-bit math to calculate elapsed time.  I measure time between sequences of rising edges, and each period is simply:

   elapased_u16t = new_timestamp_u16t - old_timestamp_u16t;  //timestamps pulled from capture register

The unsigned math will always give the proper difference, even including one rollover.  It gets 'messier' if your time period math has to include a timeframe longer than one FTM rollover, as you have to start keeping track of overflow interrupts and THOSE race conditions will give you some headaches...

0 Kudos
Reply