max DAC output frequency KV46F150M ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

max DAC output frequency KV46F150M ?

2,027 Views
matteocivale
Contributor II

Hello to everyone,

i'm looking for  the max DAC frequency output of twr-KV64F150M  board but i'dont  find it.

Can someone help me ? 

Labels (1)
0 Kudos
Reply
2 Replies

1,836 Views
soledad
NXP Employee
NXP Employee

Hello Matteo,

The Kinetis DAC output resolution is 12-bit only.

The DAC setting time is limited. For the Kinetis devices, the data sheet specifies 15–30 µs in hi-speed mode. Practical measurements have confirmed that we can go up to ~50 kHz.

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,836 Views
matteocivale
Contributor II

Thanks you  Soledad !

0 Kudos
Reply