k60f120m toggle led with onboard button

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

k60f120m toggle led with onboard button

1,645 Views
philippadolph
Contributor II

I wanted a easy start in the development with the evalutationboard. So i started to turn leds on , toggle them ....

But i can't find a simple way to toggle a onboard LED with sw1 or sw2 of of the board.

I set the systemclock

SIM_SCGC5 |= SIM_SCGC5_PORTA_MASK ;

set the sw1 as gpio

PORTA_PCR19 |= (PORT_PCR_MUX(1));

and set the resistors

PORTA_PCR19 |= PORT_PCR_PE_MASK;

If i press the button nothing happens and the GPIO_PDIR_PDI (19) don't have a high state

tmp=(GPIOA_PDIR & GPIO_PDIR_PDI(1<<19)); 

Labels (1)
0 Kudos
Reply
1 Reply

1,435 Views
mjbcswitzerland
Specialist V

Hi Philipp

I didn't see an "error" with the code but I think that you may need to add a delay between configuring the input and reading it. Don't forget that PTA19 (SW1) on the TWR board has no external pull-up resistor and the pin defaults to a XTAL output at reset. If you change its function and add a pull-up it may take a short amount of time before the input charges to '1'; if your code immediately reads the input it may always read '0', whether the button is pressed or not.

In case you want a simple start with your board see the link below since it gives you everything you may need (including industrial quality USB and Ethernet) and allows you to simulate the board in (approx.) real-time to avoid HW complications.
To do what you want in this case, the code would be (it handles all details that beginners may get wrong but gives most powerful learning and analysis capabilities at the same time)

#define SWITCH_SW1    PORTA_BIT19

_CONFIG_PORT_INPUT(A, (SWITCH_SW1), PORT_PS_UP_ENABLE); // configure the input (including clocking and characteristics)
if (_READ_PORT_MASK(A, SWITCH_SW1) == 0) { // read the state of the input
    // SW1 pressed
}
else {
    // SW1 not pressed
}

Note that there is one thing in your code that may have caused failure:
PORTA_PCR19 |= (PORT_PCR_MUX(1)); // risky but works for this pin
This works since the default peripheral function is ALT 0 (XTAL) but may fail if it weren't.
PORTA_PCR19 = (PORT_PCR_MUX(1)); // no risk

Regards

Mark

Kinetis for Professionals: http://www.utasker.com/kinetis.html
K60F120: http://www.utasker.com/kinetis/TWR-K60F120M.html