i have KDS_2.0.0 and KSDK_1.1.0 can i create a mqx project using TWR_K20D72M board.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i have KDS_2.0.0 and KSDK_1.1.0 can i create a mqx project using TWR_K20D72M board.

958 次查看
josephxavier
Contributor III

i have KDS_2.0.0 and KSDK_1.1.0 can i create a MQX  project using TWR_K20D72M board, if yes how please share the steps .

If no what all should be done in order to create a MQX  project using TWR_K20D72M board using  KDS

2 回复数

835 次查看
danielchen
NXP TechSupport
NXP TechSupport

I suggest you start from an existing MQX KDS project, and modify your code based on the project, that will be much easier.  You can start from KSDK1.2, (will be released soon), K20d72m board is still not supported yet. you can choose the closest supported board, then porting it to K20D72M

835 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello joseph,

I answered you on your service request and also I noticed, you have the same question here Re: Can we use Kinetis Software Development Kit (KSDK)  For TWR – K20D72M BOARDS . Is there any docu...

and here can any one share the steps to create MQX project for TWR_K20D72M board using KDS_2.0.0 and KSDK_1.1...

Please, is there any other issue?

Best Regards,

Iva

0 项奖励
回复