how to update a duty value of KEA128 FlexTimer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to update a duty value of KEA128 FlexTimer

Jump to solution
1,652 Views
ikkishingu
Contributor II

Hello,

I make the sample code to update a duty value of KEA128 FlexTimer during running timer count

(i.e. real time duty update),

but it doesn't work well.

This is my sample code, then could you let me know what should be modified?

Or could you provide the sample code to update a duty value?

[Condition]

PWM output : FTM2 Ch1

PWM setting mode : Edge-Aligned

Modulo : 0x000000FF(256counts)

Clock Source : system clock

[Observation]

the fisrt duty value(0x40) is effected,

but the second duty value(0x01) is not effected.

[Source Code]

--

/* global valiables */

volatile unsigned long duty = 0x00000040;

void Clk_Init()
{
        ICS_C1|=ICS_C1_IRCLKEN_MASK;   /* Enable the internal reference clock*/
while(!(ICS_S & ICS_S_LOCK_MASK));   /* Wait for FLL lock, now running at 48 MHz (1280 * 37.5Khz) */
        ICS_C2 = 0x00;    /*BDIV=1, Bus clock = 48 MHz*/
ICS_S |= ICS_S_LOCK_MASK ;    /* Clear Loss of lock sticky bit */
}

void FTM_Init()
{
SIM_SCGC |= SIM_SCGC_FTM2_MASK; /* Enable Clock for FTM2 */
       
        FTM2_MODE |= FTM_MODE_FTMEN_MASK; /* FTM2 enabled */
       
        /* Mask the output channels for safe state */
        FTM2_OUTMASK |= FTM_OUTMASK_CH1OM_MASK; /* FTM2 ch1 output mask */
       
        /* Set Modulo */
        FTM2_MOD = 0x000000FF; /* 0xFF(255) + 1 = 256 counts */

       /* Channel 1 : Edge-alined PWM */
        FTM2_C1SC |= FTM_CnSC_MSB_MASK;  /* Channel as Edge-aligned PWM mode */
        FTM2_C1SC |= FTM_CnSC_ELSB_MASK; /* High-true pulses */

        /* Set period value */
        FTM2_C1V = duty;

        /* write any value to CNT in order to reset FTM Counter and update the channels output according to new configuration */
        FTM2_CNT = 0x00000001;
       
        /* Clock setting */
        FTM2_SC |= FTM_SC_PS(0); /* Select Prescaler in this case 1. 48 Mhz /1 =48Mhz. */
        /* Counter increase by one every 20.8 ns */
        FTM2_SC |= FTM_SC_CLKS(1); /*FTM2 use system clock*/

       
        FTM2_SYNCONF |= FTM_SYNCONF_SYNCMODE_MASK; /* for PWM duty updating sync by SWSYNC */
        FTM2_SYNCONF |= FTM_SYNCONF_SWWRBUF_MASK; /* for PWM duty updating sync by SWSYNC */
        FTM2_SYNC |= FTM_SYNC_SWSYNC_MASK; /* for PWM duty updating sync by SWSYNC */

        /* Unmask the output channels */
        FTM2_OUTMASK &= ~FTM_OUTMASK_CH1OM_MASK;
       
}

void main(void)
{
 
Clk_Init();     /* Configure clocks to run at 48 Mhz */
FTM_Init();    /* Initialize the FTM module */

        FTM2_PWMLOAD |= FTM_PWMLOAD_LDOK_MASK; /* Loading updated values is enabled */
       
for(;;) {
          FTM2_C1V = duty;
          duty = 0x01; /* for updating a duty value on running */
          FTM2_SYNC |= FTM_SYNC_SWSYNC_MASK;
}

}

--

Best Regards,

Ikki

Labels (1)
0 Kudos
Reply
1 Solution
1,103 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi ikki shingu,

    Because your FTM mode is in synchronization enhanced mode, please change your code

        FTM2_C1V = duty;

          duty = 0x01; /* for updating a duty value on running */

          FTM2_SYNC |= FTM_SYNC_SWSYNC_MASK;

in for(;;) to the following code:

FTM2_COMBINE |= FTM_COMBINE_SYNCEN0_MASK;

    FTM2_SYNCONF |= FTM_SYNCONF_SWWRBUF_MASK | FTM_SYNCONF_SWRSTCNT_MASK | FTM_SYNCONF_SYNCMODE_MASK;

    FTM2_SYNC = 0x00;

FTM2_C1V = duty;
FTM2_SYNC = 0x80;// generate software trigger to change the duty value

Then you will find your FTM2_C1V changed to the new data duty.

Besides, we have an application code about this, AN4560: pwm synchronization using kinetis flextimers, the link is:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4560.pdf?fsrch=1&sr=1&pageNum=1

Wish it helps you!

If you still have question, please contact me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
1,104 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi ikki shingu,

    Because your FTM mode is in synchronization enhanced mode, please change your code

        FTM2_C1V = duty;

          duty = 0x01; /* for updating a duty value on running */

          FTM2_SYNC |= FTM_SYNC_SWSYNC_MASK;

in for(;;) to the following code:

FTM2_COMBINE |= FTM_COMBINE_SYNCEN0_MASK;

    FTM2_SYNCONF |= FTM_SYNCONF_SWWRBUF_MASK | FTM_SYNCONF_SWRSTCNT_MASK | FTM_SYNCONF_SYNCMODE_MASK;

    FTM2_SYNC = 0x00;

FTM2_C1V = duty;
FTM2_SYNC = 0x80;// generate software trigger to change the duty value

Then you will find your FTM2_C1V changed to the new data duty.

Besides, we have an application code about this, AN4560: pwm synchronization using kinetis flextimers, the link is:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4560.pdf?fsrch=1&sr=1&pageNum=1

Wish it helps you!

If you still have question, please contact me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,103 Views
ikkishingu
Contributor II

Jingjing-san,

Thanks to your advice, I can change the duty during running.

I understand settings of COMBINE[SYNCEN0] and SYNCONF[SWRSTCNT] were missing in my original code.

Thank you for your help!

Best Regards,

Ikki

0 Kudos
Reply
1,103 Views
vignesh_vb_7
Contributor IV

Where you able to update the FTM2_MOD also?

0 Kudos
Reply
1,103 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi vignesh balaji,

    Please also follow application note AN4560, then you can update the MOD register.

Wish it helps you!

Jingjing

0 Kudos
Reply