how to update a duty value of KEA128 FlexTimer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to update a duty value of KEA128 FlexTimer

ソリューションへジャンプ
2,235件の閲覧回数
ikkishingu
Contributor II

Hello,

I make the sample code to update a duty value of KEA128 FlexTimer during running timer count

(i.e. real time duty update),

but it doesn't work well.

This is my sample code, then could you let me know what should be modified?

Or could you provide the sample code to update a duty value?

[Condition]

PWM output : FTM2 Ch1

PWM setting mode : Edge-Aligned

Modulo : 0x000000FF(256counts)

Clock Source : system clock

[Observation]

the fisrt duty value(0x40) is effected,

but the second duty value(0x01) is not effected.

[Source Code]

--

/* global valiables */

volatile unsigned long duty = 0x00000040;

void Clk_Init()
{
        ICS_C1|=ICS_C1_IRCLKEN_MASK;   /* Enable the internal reference clock*/
while(!(ICS_S & ICS_S_LOCK_MASK));   /* Wait for FLL lock, now running at 48 MHz (1280 * 37.5Khz) */
        ICS_C2 = 0x00;    /*BDIV=1, Bus clock = 48 MHz*/
ICS_S |= ICS_S_LOCK_MASK ;    /* Clear Loss of lock sticky bit */
}

void FTM_Init()
{
SIM_SCGC |= SIM_SCGC_FTM2_MASK; /* Enable Clock for FTM2 */
       
        FTM2_MODE |= FTM_MODE_FTMEN_MASK; /* FTM2 enabled */
       
        /* Mask the output channels for safe state */
        FTM2_OUTMASK |= FTM_OUTMASK_CH1OM_MASK; /* FTM2 ch1 output mask */
       
        /* Set Modulo */
        FTM2_MOD = 0x000000FF; /* 0xFF(255) + 1 = 256 counts */

       /* Channel 1 : Edge-alined PWM */
        FTM2_C1SC |= FTM_CnSC_MSB_MASK;  /* Channel as Edge-aligned PWM mode */
        FTM2_C1SC |= FTM_CnSC_ELSB_MASK; /* High-true pulses */

        /* Set period value */
        FTM2_C1V = duty;

        /* write any value to CNT in order to reset FTM Counter and update the channels output according to new configuration */
        FTM2_CNT = 0x00000001;
       
        /* Clock setting */
        FTM2_SC |= FTM_SC_PS(0); /* Select Prescaler in this case 1. 48 Mhz /1 =48Mhz. */
        /* Counter increase by one every 20.8 ns */
        FTM2_SC |= FTM_SC_CLKS(1); /*FTM2 use system clock*/

       
        FTM2_SYNCONF |= FTM_SYNCONF_SYNCMODE_MASK; /* for PWM duty updating sync by SWSYNC */
        FTM2_SYNCONF |= FTM_SYNCONF_SWWRBUF_MASK; /* for PWM duty updating sync by SWSYNC */
        FTM2_SYNC |= FTM_SYNC_SWSYNC_MASK; /* for PWM duty updating sync by SWSYNC */

        /* Unmask the output channels */
        FTM2_OUTMASK &= ~FTM_OUTMASK_CH1OM_MASK;
       
}

void main(void)
{
 
Clk_Init();     /* Configure clocks to run at 48 Mhz */
FTM_Init();    /* Initialize the FTM module */

        FTM2_PWMLOAD |= FTM_PWMLOAD_LDOK_MASK; /* Loading updated values is enabled */
       
for(;;) {
          FTM2_C1V = duty;
          duty = 0x01; /* for updating a duty value on running */
          FTM2_SYNC |= FTM_SYNC_SWSYNC_MASK;
}

}

--

Best Regards,

Ikki

ラベル(1)
0 件の賞賛
返信
1 解決策
1,686件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi ikki shingu,

    Because your FTM mode is in synchronization enhanced mode, please change your code

        FTM2_C1V = duty;

          duty = 0x01; /* for updating a duty value on running */

          FTM2_SYNC |= FTM_SYNC_SWSYNC_MASK;

in for(;;) to the following code:

FTM2_COMBINE |= FTM_COMBINE_SYNCEN0_MASK;

    FTM2_SYNCONF |= FTM_SYNCONF_SWWRBUF_MASK | FTM_SYNCONF_SWRSTCNT_MASK | FTM_SYNCONF_SYNCMODE_MASK;

    FTM2_SYNC = 0x00;

FTM2_C1V = duty;
FTM2_SYNC = 0x80;// generate software trigger to change the duty value

Then you will find your FTM2_C1V changed to the new data duty.

Besides, we have an application code about this, AN4560: pwm synchronization using kinetis flextimers, the link is:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4560.pdf?fsrch=1&sr=1&pageNum=1

Wish it helps you!

If you still have question, please contact me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,687件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi ikki shingu,

    Because your FTM mode is in synchronization enhanced mode, please change your code

        FTM2_C1V = duty;

          duty = 0x01; /* for updating a duty value on running */

          FTM2_SYNC |= FTM_SYNC_SWSYNC_MASK;

in for(;;) to the following code:

FTM2_COMBINE |= FTM_COMBINE_SYNCEN0_MASK;

    FTM2_SYNCONF |= FTM_SYNCONF_SWWRBUF_MASK | FTM_SYNCONF_SWRSTCNT_MASK | FTM_SYNCONF_SYNCMODE_MASK;

    FTM2_SYNC = 0x00;

FTM2_C1V = duty;
FTM2_SYNC = 0x80;// generate software trigger to change the duty value

Then you will find your FTM2_C1V changed to the new data duty.

Besides, we have an application code about this, AN4560: pwm synchronization using kinetis flextimers, the link is:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4560.pdf?fsrch=1&sr=1&pageNum=1

Wish it helps you!

If you still have question, please contact me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,686件の閲覧回数
ikkishingu
Contributor II

Jingjing-san,

Thanks to your advice, I can change the duty during running.

I understand settings of COMBINE[SYNCEN0] and SYNCONF[SWRSTCNT] were missing in my original code.

Thank you for your help!

Best Regards,

Ikki

0 件の賞賛
返信
1,686件の閲覧回数
vignesh_vb_7
Contributor IV

Where you able to update the FTM2_MOD also?

0 件の賞賛
返信
1,686件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi vignesh balaji,

    Please also follow application note AN4560, then you can update the MOD register.

Wish it helps you!

Jingjing

0 件の賞賛
返信