high-current drive MKE04Z128VLD4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

high-current drive MKE04Z128VLD4

ソリューションへジャンプ
1,741件の閲覧回数
jun1
Contributor V

Thank you for helping.

1. MKE04Z128VLD4 44pin is used.

    As you can see, does this package support high current output?

2. “8 PINOUT” in the MKE04P80M48SF0 manual stated “PTB4, PTB5, PTD0, PTD1, PTE0, PTE1, PTH0, and PTH1 are high-current drive pins when operated as output.”
I thought I could use that function.

3. In the notes of `` 5.1.1 DC characteristics '', `` 2. Only PTB4, PTB5, PTD0, PTD1, PTE0, PTE1, PTH0 (64-pin and 80-pin packages only), and PTH1 (64-pin and 80- pin packages only) support high current output. "
I found that description after creating the board.


I think it ’s very unfriendly.

So far, complaints about confirmation and manual unkindness.

jun.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,657件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi jun,

MKE04Z128VLD4 really has high current pin. PTB4, PTB5, PTD0, PTD1, PTE0, PTE1 still are high current pins.

"Only PTB4, PTB5, PTD0, PTD1, PTE0, PTE1, PTH0 (64-pin and 80-pin packages only), and PTH1 (64-pin and 80- pin packages only) support high current output. "

I have to say this sentence looks have problem. I'm sorry for that.

Regards,

Jing

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,658件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi jun,

MKE04Z128VLD4 really has high current pin. PTB4, PTB5, PTD0, PTD1, PTE0, PTE1 still are high current pins.

"Only PTB4, PTB5, PTD0, PTD1, PTE0, PTE1, PTH0 (64-pin and 80-pin packages only), and PTH1 (64-pin and 80- pin packages only) support high current output. "

I have to say this sentence looks have problem. I'm sorry for that.

Regards,

Jing

0 件の賞賛
返信
1,657件の閲覧回数
jun1
Contributor V

Thank you for your teachings. It is said that Japanese is difficult to understand because the subject is ambiguous, but English has a similar situation. understood. PTH is not a 44-pin type. The understanding was shallow. Other than that, I was relieved to know that it was a 44-pin type.

jun.

0 件の賞賛
返信