freesrtos+MMAU+KM34Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,783件の閲覧回数
nickng
Contributor II

Hi ,

If I want to use the freeRTOS with MMAU in a KM34Z MCU. Do I need to some port.c modification in order to use MMAU without troubles?

e.g the store /restore the MMAU registers?

Thanks!

ラベル(1)
タグ(4)
1 解決策
4,186件の閲覧回数
MarMi
NXP Employee
NXP Employee

Hi Nick,

from MMAU initialization point of view as Jing explained above - no special steps needed.

Yes MMAU register context save / restore would have to be handled by FreeRTOS if MMAU is used in more tasks. In this case, most likely, portasm.s would have to be be extended by saving/restoring MMAU registers.

If you plan using MMAU in single task then no saving/restoring MMAU is required and use can use current FreeRTOS files

Kind regards,

Martin M. 

元の投稿で解決策を見る

4 返答(返信)
4,187件の閲覧回数
MarMi
NXP Employee
NXP Employee

Hi Nick,

from MMAU initialization point of view as Jing explained above - no special steps needed.

Yes MMAU register context save / restore would have to be handled by FreeRTOS if MMAU is used in more tasks. In this case, most likely, portasm.s would have to be be extended by saving/restoring MMAU registers.

If you plan using MMAU in single task then no saving/restoring MMAU is required and use can use current FreeRTOS files

Kind regards,

Martin M. 

4,186件の閲覧回数
nickng
Contributor II

HI Martin,

Thanks or the answer.

By the way, the FreeRTOS embedded most os the asm code in port.c as well.

0 件の賞賛
返信
4,186件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Nick,

No, you do not need to do any thing to enable MMAU. To minimize power dissipation, the design supports an architectural clock gate for the entire module, that is, the MMAU is only clocked when responding to bus requests to its programming model or is busy performing a calculation.

There is a MMAU demo in KM34 sdk, please find it in \boards\twrkm34z75m\driver_examples\mmau.

Regards,

Jing

0 件の賞賛
返信
4,186件の閲覧回数
nickng
Contributor II

Hi Jing,

Thanks for your reply!

My question is focusing on the context switching ( or interrupts) of the RTOS with that specific MMAU registers.

For a bare metal system, with can use the pair of store and restore action of those mmau register. Do I need to do the same on the port.c ? 

here are the store/restore pair :

pastedImage_1.png

0 件の賞賛
返信